How to export a high resolution PNG file

2019-05-15T15:37:01Z

Summary


Details

How to export a high resolution PNG file.



Solution

 Each of the File Export commands (PNG/JPEG/TIFF/etc.) creates a raster image 
from the graphics window and saves the image in the specified format. The 
resolution of the image is always the same as the resolution of the graphics 
window.


If a Drafting user wishes to export a raster image with greater resolution, 
they can use 'File-->Plot'. Plot supports PNG/JPEG/TIFF "printers" that convert 
CGM output to an image in the specified format. 
1. Open the drawing sheet. 
2. Select 'File-->Plot'. 
3. In the Plot dialog, under the Actions group, select 'Advanced Plot'. 
4. Select the 'Printer' tab. 
5. In the Select Printer/Profile group, set 'Printer/Output Format' to 
 'PNG Export File'. 
6. Select the 'Print Setup' tab. 
7. Specify the desired resolution in the Print Dimensions group. 
8. Select the 'Print' button at the bottom of the dialog. 
9. Specify a name for the PNG file.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V7.5
Function: VISUALIZATION

Ref: 001-7108555

KB Article ID# PL8010904

Contents

SummaryDetails

Associated Components