MOM variable to determine Motion Output setting in Drilling operation

2019-05-08T11:56:33Z

Summary


Details

When using a Drilling operation there is a Motion Output setting with the values "Machine Cycle" or "Single Moves". Is there any MOM variable that can be used in the post processor to determine the selected value?



Solution

Try using the variable mom_cycle_definition_mode. If the setting is "Machine Cycle" the value is 0 and if the setting is "Single Moves" the value is 1.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: CAM
Version: V10.0.3
Function: POSTPROCESS

Ref: 001-7792738

KB Article ID# PL8010898

Contents

SummaryDetails

Associated Components