Drilling operation drills hole oversize without warning

2019-11-01T13:40:35Z

Summary


Details


Drilling operation drills hole oversize without warning.



Solution

We do allow oversize machining, so this is as expected. 
When we generate a drilling operation with an oversize tool, there will be an alert:


"Tool Diameter is greater then Feature Diameter. Tool will gouge part."


Note that the alert will only appear once. If the operation is regenerated, there will not be an alert. This is as designed.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: n/a
Product: NX
Application: CAM
Version: V11.0.1
Function: DRILLING

Ref: 001-7962117

KB Article ID# PL8010893

Contents

SummaryDetails

Associated Components