A series of
UDE's were added to an operation in the
Machine Control Start or
End of Path Events in one operation and need to be copied to a second. The
UDE's in the source operation might look something like the picture below.

Solution
To copy the group of
UDE's from one operation to a different operation in the same part, select
Machine Control(Pane) -> Copy from... -> From -> Operation and click the operation to copy from.


If a second part file is opened as a template then this file will be listed when
Machine Control(Pane) -> Copy from... -> From -> Template is selected.

Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V1859
Function: BASIC_FUNCTIONS
Ref: 001-8845866