GRIP is a relatively old programming language. Are there any plans to stop the support of GRIP in a future NX version?
Solution
Currently there are no plans to stop the support of GRIP. The product is not actively enhanced, but bug fixes are still done to make sure that the existing functionality works. There are still a lot of customers who use GRIP programs and depend upon them.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: VIST32P1
Product: NX
Application: SYSENG
Version: V10.0
Function: UG/OPEN
Ref: 001-7340650