Where is the Resource Bar Multiple Windows option in NX9?

2019-08-28T15:01:15Z

Summary


Details

--------------- 
Where is Resource bar Multiple Windows option in NX9?



Solution

 1. Go to Menu --> Preferences --> User Interface --> Layout tab.


2. Change the Display Resource Bar setting to As Ribbon Tab --> OK 


3. Menu --> Tools --> Customize --> Commands tab


4. From the Categories column --> Expand All Tabs --> Expand Resource Bar.


6. Select Resource Bar.


7. In the Commands column, Multiple Windows is available



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 764
Product: NX
Application: SYSENG
Version: V9.0
Function: UI_TOOLS

Ref: 001-7155211

KB Article ID# PL8010879

Contents

SummaryDetails

Associated Components