Quicker selection adding Sketcher Geometric Constraints in NX 8.5

2019-08-28T15:00:56Z

Summary


Details

--------------- 
Some users going to NX 8.5 feel that adding Sketch Geometric Constraints is 
more cumbersome than previous versions by having to open the Geometric 
Constraints menu, selecting the Constraint type, then selecting the curves. Is 
there a quicker way in NX 8.5?



Solution

 NX 8.5 also introduced the "Sketch Shortcut Toolbar" that will eliminate the 
need to open the Geometric Constraints menu. 


For example, with 2 perpendicular lines, if you select the end point of one 
line and then select the other line, and the constraint options for Point On 
Curve / Mid Point / Fixed would be raised. If you select a Circle and a Line 
you will get the options for Tangent / Perpendicular / Fixed / Fully Fixed.


Also, note that where you select the curves will make a difference what 
constraint options are available.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 764sp1
Product: NX
Application: DESIGN
Version: V8.5
Function: SKETCHER

Ref: 001-6919567

KB Article ID# PL8010878

Contents

SummaryDetails

Associated Components