Catia to NX Translation does not include wireframe curves

2019-08-28T15:01:12Z

Summary


Details

--------------- 
Opening a Catia (catpart) file into NX, Only the solid bodies are getting 
translated in. How can you include the wireframe data in the translation?



Solution

 The setting for Include No Show Entities needs to be toggled ON.


When using "File --> Open", select the [Options] button in the lower left hand 
corner of the Open dialog and toggle ON the option Include No Show Entities.


To toggle the option ON by default, edit the catiav5.def file, change the 
setting to be ON.


When importing the CATIA catpart file into an NX part file using File --> 
Import --> Catia V5.. there's an option to toggle ON Include No Show Entities 
in the Import Catia V5 dialog.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: TRANSLATOR
Version: V9.0
Function: CATIAV5

Ref: 001-7614565

KB Article ID# PL8010877

Contents

SummaryDetails

Associated Components