How to find the installed version of Siemens PLM Licensing

2020-08-20T22:25:12Z

Summary


Details

Is there a way to determine the installed version of Siemens PLM Licensing from the server and from the NX workstation?



Solution

Yes, there are methods for finding the installed version of Siemens PLM Licensing from the server and from the client. The examples below show that Siemens PLM Licensing 11.0 is installed.

1.  On the license server system


Locate the file 'VERSION.TXT' in the installation folder for Siemens PLM Licensing (default location is C:\Program Files\Siemens\PLMLicenseServer) 


For example:

VERSION.TXT
Siemens PLM License Server
11.0.0.7



2.  On the NX workstation via Licensing Tool.  For example:

Start --> All Apps --> Siemens NX --> Licensing Tool --> Environment Settings

License Server 
License Server: 28000@barney


28000@barney
Connection Status: Successful
Sold To ID: xxx4567
Webkey: ABC123DEF4
Issuer: SIEMENS
Version: 11.16 (FlexNet Publisher version of the server)
Siemens Licensing Version: 11.0



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: SYSENG
Version: V1926
Function: SYSTEM_TOOLS

Ref: 001-7221746

KB Article ID# PL8010876

Contents

SummaryDetails

Associated Components