How to remove certain features from a Flat Pattern

2019-05-15T15:36:46Z

Summary


Details

How to create a 'Flat Pattern' Sheet Metal feature and exclude certain 
features.



Solution

 Currently NX does not have the functionality to exclude certain features from 
the Flat Pattern feature. However, if the features to remove are at the end of 
the Part History, an extracted body can be created in order to build the Flat 
Pattern. 
1. Expand the Part Navigator and use 'MouseButton3-->Make Current Feature' on 
the last feature to be included in the Flat Pattern. 
2. Create an Extracted Body using the 'Fixed at Timestamp' option. 
3. Select the Extracted Body to create the Flat Pattern feature. 
The Flat Pattern created from the extracted body will not contain any features 
created after the Extracted Body feature.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NX_SHEET_METAL
Version: V9.0
Function: FLAT_PATTERN

Ref: 001-7736454

KB Article ID# PL8010873

Contents

SummaryDetails

Associated Components