Close Assembly Clearance shows hard interference value not exact

2019-05-22T13:39:08Z

Summary


Details

Assembly Clearance analysis not producing accurate hard interference distance value. 

Is there a way to configure the accuracy of this value?



Solution

Per NX Help Documentation: Home> CAD > Assemblies > Advanced assembly commands > Representations, it states that representations are used with Clearance Analysis.


This means the tolerance values for representation of the bodies in the components will determine the accuracy of the calculated interferences distance value.


Use the following steps to modify the tolerance of a representation: 

1. Make each of the components involved in the Assembly Clearance analysis the Display Part 

2. Use "menu >Assemblies > Advanced > Representation": 
Click on "Edit Facet Parameter". 
Highlight body (or the name of the representation in the list). OK 

3. In the Edit Facet Parameters dialog, change the value for Distance Tolerance and Angle Tolerance. Try these values: 
Distance = 0.001 
Angle = 0.5
 
4. OK the dialog. 
Repeat for all components involved.
 
5. Run the Assembly Clearance analysis by executing "Perform Analysis" on that existing SET, examine the Interference distance value, this should become more accurate.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764SP1
Product: NX
Application: ASSEMBLIES
Version: V10.0.3
Function: ASSEMBLY_MODEL

Ref: 001-7957226

KB Article ID# PL8010868

Contents

SummaryDetails

Associated Components