There is no Angular option to rotate a drawing view

2019-05-15T15:36:02Z

Summary


Details

Unable to rotate a drafting view that contains a View Break.



Solution

 If the drawing view has a View Break applied to it, the Angle option is removed 
from the View Settings, preventing the view from being rotated. 
1. Hover the cursor over the view border, 'MouseButton3-->Settings'. 
2. Expand 'Common' and highlight 'Angle'. 
3. If no 'Angle' option is available, the View Break will have to be deleted. 
4. 'Cancel' the Settings dialog. 
5. In the Part Navigator, expand the view to rotate and delete the View Break. 
6. Repeat steps 1-2 to enter a new angle value for the drafting view. 
7. OK the Settings dialog. 
8. Recreate the View Breaks on the rotated view.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V9.0
Function: DRAWING/VIEW

Ref: 001-7716565

KB Article ID# PL8010865

Contents

SummaryDetails

Associated Components