When installed NX11.0.1 opening a SE assembly wanted to reinstall NX11

2019-05-27T09:02:05Z

Summary


Details

--------------- 
NX11.0.1 breaks Solid Edge ST9:


When opening or creating files in Solid Edge, Solid Edge crashes or this 
message comes up:


Please wait while Windows configures Siemens NX 11.0


This is the case after updating to NX11.0.1, no problem bevor this.



Solution

 - Start a Windows Command Prompt (DOS BOX) 
- Navigate into the NX installation folder 
-- enter "c:" or "d:" to change the drive letter 
-- enter "cd\" to jump into the root folder 
-- enter "cd foldername" to change into the folder with the given name 
-- enter "dir" to review the folder you are in 
-- each line in the dos box must be finished by the "enter" key


- change to the NXBIN sub-directory inside the NX installation folder 
- the installation out of the box can be found here: C:\Program 
Files\Siemens\NX 11.0\NXBIN\ , but can vary in your installation


- type in followed by "enter" key: 
regsvr32 NXCam_64.dll


- restart Solid Edge


****************



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764SP1
Product: NX
Application: SYSENG
Version: V9.0.3
Function: INSTALL_ISSUES

Ref: 001-7971362

KB Article ID# PL8010860

Contents

SummaryDetails

Associated Components