How do you change the location of temp directory the NX to JT translator uses?

2019-07-24T13:09:00Z

Summary


Details

We are opening a NX command prompt and in that prompt we define a path for the user's temp directory:


set temp=\\ServerName\Temp


We run our command against run_ugtopv.bat but the translator's log file is still writing to a different user temporary directory. How do we control where this log file is written to?



Solution

The NX to jt translator only recognizes the use of tmp, not temp, when defining a temporary directory for the log file to be written to. This behavior is most likely due to it being a Unix only application when it was 
first developed.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 2008_R2
Product: NX
Application: TRANSLATOR
Version: V10.0.2
Function: NX_JT

Ref: 001-7629970

KB Article ID# PL8010858

Contents

SummaryDetails

Associated Components