Adding a new drawing using Sheet Template and nothing happens

2019-08-28T15:00:59Z

Summary


Details

--------------- 
When attempting to add a new drawing sheet using a Sheet Template nothing 
happens and a new drawing sheet is not created.



Solution

 Open the part file that is being used for the drawing template and verify that 
the drawing sheet Units matches the Units for the template.


For example for an inch Template;


File --> Open --> "my_new_template.prt". Use "Edit --> Sheet --> Settings" 
verify that "Inches" is toggled ON to match the Template units set to English.


 <PaletteEntry id="d1"> 
 <References/> 
 <Presentation name="A - Size" description="NX Example Sheet"> 
 <PreviewImage type="UGPart" location="drawing_template.jpg"/> 
 </Presentation> 
 <ObjectData class="SheetTemplate"> 
 <TemplateFileType>none</TemplateFileType> 
 <Filename>My_new_tempalate.prt</Filename> 
 <Units>English</Units>



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 764sp1
Product: NX
Application: DRAFTING
Version: V8.0
Function: AUTOMATION

Ref: 001-6929985

KB Article ID# PL8010852

Contents

SummaryDetails

Associated Components