Simcenter 3D Solutions NX Nastran Topology Optimization (NXN 016)

2019-05-08T17:45:39Z
Simcenter 3D

Summary


Details

--------------- 

How can a user activate NX Nastran Topology Optimization (NXN016) from NX or 

Simcenter?

Solution

 To use NX Nastran Topology Optimization in SC 11, users have to take a step to 

have the controls appear in the ribbon. Here is what needs to be done:

1. RMB in an empty area of the ribbon and activate the standard Optimization 

tab. Out of the box, this tab contains 3 active groups (Optimization, Checks 

and Information, Utilities). There is a fourth group (NX Nastran Topology 

Optimization Group) that is off by default. 

2. LMB on the far right hand side of the ribbon (Ribbon Options - highlighted 

in blue below). Toggle on the "NX Nastran Topology Optimization Group"

User should end up with a 4th optimization group on the optimization ribbon 

bar which contains 2 icons (Setup and Post Processing).

Notes

KB Article ID# PL8010849

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow