Machining Knowledge file saved in incorrect encoding

2019-11-04T08:56:29Z

Summary


Details

Warning on each launch of NX where following message is displayed:


WARNING: Your machining knowledge file was saved using an incorrect XML encoding ('ISO-8859-1').


machining knowledge file: 
'C:\NX10\mach\resources\machining_knowledge\machining_knowledge.xml'


This may have a negative impact on the display of multi-byte characters for non-English languages. 
It is highly recommended that you Open and Save your machining knowledge file using the Machining Knowledge Editor to fix this issue.



Solution

 Suspected the .xml had been opened and saved in a different editor


Resolved by:


open the .xml file with 'start - all programs - Siemens NX10 - Manufacturing - Machining Knowledge Editor'


Save


(This is the info we should see at the file header)


<?xml version="1.0" encoding="UTF-8" standalone="true"?> 
<Data PpXmlVer="10.0"><Objects><PmProject 
ExternalId="OOTB_Project"><NodeInfo><Id>1</Id>



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: n/a
Product: NX
Application: CAM
Version: V10.0.3
Function: FEATURE_BASED

Ref: 001-7606190

KB Article ID# PL8010846

Contents

SummaryDetails

Associated Components