PMI does not display in correct colors in wireframe mode

2019-05-15T15:35:53Z

Summary


Details

PMI appears as dimmed or grayed out when using the rendering style 'Wireframe 
with Hidden Edges'. 
The PMI dimensions appear dimmed when they are hidden by the solid body and 
will not display correctly in screen captures.



Solution

 1. Select 'Preferences-->Visualization'. 
2. Select the 'Color' tab. 
3. Set the 'Hidden Geometry' color to be the same as the PMI default color.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Function: DISPLAY

Ref: 001-6812146

KB Article ID# PL8010839

Contents

SummaryDetails

Associated Components