When running an NXOpen program, the session returns the following error in the syslog: PK_ERROR_tag_limit_exceeded
Solution
This is a potential limitation of the Parasolid Kernel; there are roughly 2.5 billion tags available in the Parasolid Kernel. Unfortunately these tags are not reused and the potential exists to run out of available tags in the NX session. Currently, the only workaround is to save and close the part and reopen it, which should release all tags for use again.
Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V1953
Function: NXOPEN
Ref: 001-8952626