Solid Edge part will not open in NX

2019-11-04T08:55:19Z

Summary


Details

Unable to open Solid Edge '.par' file. Get error "The specified string contains a syntax error"



Solution

problem is caused by an attribute on the Solid Edge part:


Having a value of ~ 


The ~ is causing the problem, so if it can be removed on the SolidEdge side, then the part would load.


This is fixed in NX 11.0, and NX 10.0.2



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V10.0.1
Function: PART_FILE_OPS

Ref: 001-8268561

KB Article ID# PL8010830

Contents

SummaryDetails

Associated Components