---------------
A
Planar Mill Operation is edited and the
Select or Edit the Part Boundaries icon is selected. Why is the
List pane not displayed allowing the available
Boundaries to be edited or deleted?
Solution
The
Collapsed List pane is hidden. In the upper left corner of the
Select or Edit the Part Boundaries menu, select the gear shaped icon. Select
Show Collapsed Groups in order to display all panes.
Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: P1899
Function: USER_INTERFACE
Ref: 001-7957217