Modifying the Prefix for View Labels

2019-05-15T15:35:45Z

Summary


Details

View Label Prefix in a custom drafting standard does not recognize an empty space



Solution

 1. Select 'File-->Utilities-->Customer Defaults'. 
2. Expand 'Drafting'. Highlight 'General'. 
3. Select the 'Standard' tab. 
4. Select the 'Customize Standard' button. 
5. Highlight 'View Label'. 
6. Under each of the tabs, there is a field to enter a 'Prefix' 
 for the 'View Label'. 
7. If no Prefix is desired enter a set of double quotation marks, "", 
 or use the space bar to enter a space in the field. 
8. The default 'Prefix' can also be used, or enter a custom 'Prefix'. 
9. Once the 'Prefix' fields have been modified, select 'Save' on the 
 Customized Drafting Standard dialog. 
10. Select 'Cancel' to go back to the Customer Defaults dialog. 
11. OK the Customer Defaults dialog. 
12. Restart a new session of NX for the changes to take effect.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: GATEWAY
Version: V8.0
Function: CUSTOMER_DEFS

Ref: 001-7113197

KB Article ID# PL8010815

Contents

SummaryDetails

Associated Components