How can existing Exploded Views in an assembly be viewed using NX Viewer?

2019-05-15T17:23:38Z

Summary


Details

How can existing Exploded Views in an assembly be viewed using NX Viewer?



Solution

 In NX, each Exploded View can be assigned to a different Model View. Then in 
NX Viewer, the different Model Views can be made active to display the active 
Explosion in each Model View.


In NX: 
1. Open the assembly that contains the existing Explosions. 
2. Select 'Assemblies-->Exploded Views-->Show Toolbar' to display the 
 Exploded Views toolbar. 
3. In the Part Navigator, expand 'Model Views'. 
4. In the Part Navigator, select 'Model Views', 
 'MouseButton3(MB3)-->Add View'. 
5. Name the view the same name as one of the Exploded Views. 
6. If the new Model View did not automatically become the active work view, 
 double-click on the new Model View to make it the work view. 
7. In the Exploded Views toolbar, toggle to the Exploded View by the 
 same name as the active Model View. 
8. Repeat steps 4-7 for each Exploded View in the assembly. 
9. Once a Model View has been created for each Exploded View and each 
 Model View has been assigned its corresponding Exploded View, 
 select 'File-->Save' to save the assembly file.


In NX Viewer: 
1. Open the assembly. 
2. In the Part Navigator, expand 'Model Views'. 
3. Double-click a Model View to make it the active work view. 
 The Exploded View assigned to this Model View will be displayed.


Now different Model Views can be made active in NX Viewer to see each of the 
Exploded Views.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ARCHITECTURE
Version: V8.5
Function: NX_VIEWER

Ref: 001-6914410

KB Article ID# PL8010812

Contents

SummaryDetails

Associated Components