Simcenter 3D Solutions Fatal Error in Coupled Thermal-Flow Solution

2019-11-04T09:16:02Z
Simcenter 3D

Summary


Details

Fatal Error in Coupled Thermal-Flow Solution

Unable to perform an (advanced) coupled thermal-flow solution because of a fatal error during the solve of the thermal model:

"QProcess Error: cannot validate module version File SCX34 not found"

Solution

The error usually appears when: 

* The simulation was aborted but continues to run in the background. 

* The virus scanner is checking the files as the run is being executed.

The second is the most likely cause of this problem. To solve this, make sure no solver processes are running in the background or restart the computer. 

Disable the virus scanner for the directory where the files are placed, and make sure the Anti-virus is is not checking the executables in the TMG folder.

Notes

KB Article ID# PL8010810

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow