In the Turning module after you run a part-off operation the system does not track the stock on the end of the part that has been parted off when you use "From Workspace" to define the Blank for the second work side, if it is the smaller portion of the blank that is remaining.
Solution
This is currently as designed
"From Workspace" tracks the larger piece of the blank stock
- regardless of whether this is the remaining piece in the chuck or the piece cut off.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: n/a
Product: NX
Application: CAM
Version: V10.0.2
Function: VERIFY
Ref: 001-8285737