How to add crosshatch to model curves

2019-05-15T15:35:35Z

Summary


Details

How to add crosshatch to model curves



Solution

To apply crosshatch to letters/curves, perform the following:


1.  Start the drafting application


2.  If there is not a sheet present in drafting, hit cancel on the Sheet 
     dialog


3.  If there is a sheet present, the Display Sheet command will need to be 
     executed 


4.  Start the crosshatch command and set the Curve Rule to Connected Curves


5.  Select the curves/letters individually and apply the crosshatch


Note:  If for some reason connected curves are not selectable, reset the 
            dialog memory in the Crosshatch dialog box



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V10.0.3
Function: DRAWING/VIEW

Ref: 001-8931014

KB Article ID# PL8010790

Contents

SummaryDetails

Associated Components