How to dismiss the 'Set Mirror Plane' command

2019-05-15T15:34:58Z

Summary


Details

How to turn off the display of the dynamic coordinate system (csys) Mirror 
Plane in the 'Set Mirror Plane' command.


When the 'View-->Operation-->Set Mirror Plane' command is active there is a 
dynamic csys. When the csys has been properly oriented, there is no dialog to 
allow the user to select 'OK' to complete the command and remove the display of 
the dynamic csys.



Solution

 Select MouseButton2 (MiddleMouseButton) to complete the command and the 'Set 
Mirror Plane' dynamic csys will be removed from the display.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Function: DISPLAY

Ref: 001-7228886

KB Article ID# PL8010780

Contents

SummaryDetails

Associated Components