NX The Delete Face dialog is missing the 'Blend Size' option.

2019-05-15T15:34:43Z
NX for Design

Summary


Details

In the Delete Face dialog in the Type group, the listing for 'Blend Size' is 
missing.



Solution

 The 'Blend Size' option will not be available in the Delete Face dialog if the 
environment variable, UGII_DMX_NX502=1, is set.


Remove the UGII_DMX_NX502 environment variable from the NX environment to 
enable the ability to set the Delete Face type to 'Blend Size'.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V9.0
Function: SYNC_MODEL

Ref: 001-7202792

KB Article ID# PL8010777

Contents

SummaryDetails

Associated Components

Modeling