Using Visual reporting, Creating a report ends up with an empty window

2019-11-01T13:36:06Z

Summary


Details

Using Visual reporting, Creating a report ends up with an empty window, and an 
error in the syslog.


=============================================================================== 
&MACRO CUSTOM 29 NX_VISUAL_REPORTING * TILELIST_TYPE * MENUPOPUP * 3 ! 
&MACRO FOCUS CHANGE IN 1 
&MACRO DYN_POP_TOGGLE 4 1 "" ! Create HTML Report 
IMAGE STATUS : Generating the Image... 
C:\Users\<user>\AppData\Local\Temp\visual_reporting_html_results\html_report_abcd21E0970B4ns1\html_results.png 
... 
... 
WEB BROWSER: Navigating to: 
file:///C:/Users/<user>/AppData/Local/Temp/visual_reporting_html_results/html_report_abcd21E0970B4ns1/index.html 
JavaScript Console Message: ReferenceError: Can't find variable: jQuery 
Line number: 5 
... 
... 
=============================================================== 
The index.html and other files are created in the temp folder, so it's not that they are missing. 
The NX browser, just stays empty, with no visible error, nor message.


For the same user, on the same system, it does work for NX 10.0 just not for NX 11.0


Steps to Duplicate: 
- Open any (small) assembly 
- Start Visual reporting 
- Select any Report that gives a result, like "Part Family member" or "part material" 
- run the Report 
- Right Click in the Results are, and select: "Create HTML Report" 
- Now the web browser tab opens, but no results, just an empty window.



Solution



The problem is caused by incompatible file versions. 


The workaround is to delete the HTML report cache folder. If you have never defined the HTML Report Output Directory, the cache folder location is:


"C:\Temp\visual_reporting_html_results". 


If you have defined the HTML Report Output Directory in customer defaults: 


"Gateway --> Visual Reporting --> General --> HTML Report Output Directory".


Or if you have defined it on the HD3D Visual Reporting Gadget dialog: 


"HD3D --> Visual Reporting --> Setting --> HTML Report Output Directory".


Then you should locates the folder accordingly and delete it.



Notes and References

PR 8329884

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: GATEWAY
Version: V11.0
Function: VISUALREPORTING

Ref: 001-8331402

KB Article ID# PL8010771

Contents

SummaryDetails

Associated Components