How to create a registered trademark as text

2019-05-15T15:34:31Z

Summary


Details

How to create and extrude the registered trademark symbol, which is the 
letter "R" with a circle around it.



Solution

 This symbol can be copied and pasted from a Microsoft Word document: 
1. Open a new document in Microsoft Word. 
2. Place the cursor in the new document. 
3. On the keyboard, perform an 'alt+cntrl+r'. 
 The registered trademark symbol is created in the document. 
4. Highlight the registered trademark symbol. 
5. On the keyboard, perform a 'cntrl+c' to copy the symbol. 
6. In NX, open a part or create a new part. 
7. Switch to the Modeling application. 
8. Select 'Insert-->Curve-->Text'. 
9. In the dialog, under the Text Properties group, place the cursor 
 in the text field. 
10. On the keyboard, perform a 'cntrl+v' to paste the registered trademark 
 symbol into the field. 
11. Complete the desired fields and options in the Text dialog. 
12. OK the Text dialog. 
The registered trademark is placed in the part and can be selected for 
Extrusion.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V7.5
Function: CURVE

Ref: 001-6990391

KB Article ID# PL8010768

Contents

SummaryDetails

Associated Components