How to configure the order of modules on the Full Screen toolbar.

2019-05-15T15:34:27Z

Summary


Details

How to configure the order of modules on the Full Screen toolbar.



Solution

 1. While in Full Screen mode, in the toolbar header,  'MouseButton3-->Customize'. 
2. While the 'Customize' dialog is open, select any of the menu choices 
 in the Full Screen toolbar (ie. 'Drawing', 'Sketch Tools', 'Standard', 
 etc.) 
 NOTE: Two green arrows will display above the menu choice. 
3. Select the green arrows to move the module to the left or to the right 
 along the top of the default toolbar. 
4. When finished, select 'Close' on the Customize dialog.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V7.5
Function: UI_TOOLS

Ref: 001-6916582

KB Article ID# PL8010764

Contents

SummaryDetails

Associated Components