3DConnexion spaceball only works in the primary view window after running a
'Model Compare'.
The 'Model Compare' function in NX will split the screen into 3 views. The
standard mouse will dynamically pan and rotate in each of the 3 views. Since
the spaceball only works in the primary view, how can the spaceball also work
in each view?
Solution
If the view window is made active, the spaceball will pan and rotate in that
view. To change the active view window, click in the view and perform a
'MouseButton3-->Work View'. The spaceball will now work in that view.
Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V8.0
Function: INFO_ANALYSIS
Ref: 001-7245597