How to move a component in relation to an existing WCS

2019-05-15T15:34:23Z

Summary


Details

How to move an existing component in relation to the Work Coordinate System 
(WCS) in the work part.



Solution

 1. Hover the cursor over the component to reposition, 'MousButton3-->Move'. 
 The Dynamic WCS will display in the work area and the 
 Move Component dialog will display. 
2. On the Move Component dialog, set "Motion = Dynamic". 
3. In the work area hover the cursor over the cone shape at the end of the 
 X, Y, or Z axis on the Dynamic WCS. 
4. After it highlights, 'MB3-->Snap Handle to WCS'. 
The Dynamic WCS will now be aligned to the WCS of the work part. Now the 
component can be moved along the X, Y, or Z axis of the Dynamic WCS for 
repositioning.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V6.0
Function: POSITIONING

Ref: 001-6366927

KB Article ID# PL8010762

Contents

SummaryDetails

Associated Components