Simcenter 3D Solutions How to plot Motion functions in NX11 Motion

2019-05-08T17:41:14Z
Simcenter 3D

Summary


Details

--------------- 

How can I plot Motion functions in NX11?

Solution

 Users can graph Motion functions by performing the following steps:

1. Open XY Results View (The window viewer sits below the Motion Navigator) 

2. Left Click and Highlight the Motion Simulation in the Motion Navigator 

3. The associated Motion functions will display in the XY Results View 

4. Right Mouse Click on a function to either Plot, Create a Graph Object, or 

Set as X Axis. 

5. Plot or Create a Graph Object will allow the user to Plot the function 

over time as well as save it to an AFU.

Notes

KB Article ID# PL8010756

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow