NX Maximum and minimum facing diameter parameters.

2019-05-15T15:34:20Z
NX for Manufacturing

Summary


Details

When defining a face groove tool, the More tab has these parameters:


Minimum Facing Diameter 
Maximum Facing Diameter


How are they used in tool path generation? The real tool has hard limits to the groove geometry where it will fit and how it can be used.



Solution

Currently, the Maximum Facing Diameter and Minimum Facing Diameter values for a face groove tool are used by NX only to produce a warning message during tool path generation. For example:


 The maximum facing diameter value of 60.00 mm has been exceeded 
 in operation 'FINISH_BORE_ID' for tool 'FACE_GROOVE_L' by 24.71 mm.


The software does not stop generating the path or trim it to these tool parameters entered in the tool definition.  It is up to the user to note the warning and manually alter the operation to ensure the tool operates within its envelope.


===============================================================================


Minimum Facing Diameter 
 
This is the minimum diameter that the tool can cut when grooving on the face of the part (trepanning) that will not cause interference on the outside of the tool. 



Maximum Facing Diameter 
 
This is the maximum diameter that the tool can cut when grooving on the face of the part (trepanning) that will not cause interference on the inside of the tool.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V10.0.3
Function: TURNING

Ref: 001-7785302

KB Article ID# PL8010751

Contents

SummaryDetails

Associated Components

Manufacturing General