Extension Lines do not allow different overhang

2019-05-15T17:21:45Z

Summary


Details

How to modify the 'Overhang' of one extension line without affecting the 
'Overhang' of the other extension line in a Linear dimension.



Solution

 1. Double-click the dimension to edit it. 
 There will be hotspots displayed on the dimension to allow for different 
 elements of the dimension to be individually edited. 
2. Select the Extension Line hotspot on the extension line that will be 
 modified. 
 This will display one arrow on both ends of the extension line. 
3. Select the arrow that controls the Overhang. 
4. In the pop-up dialog, toggle OFF 'Synchronize Both Sides'. 
 This looks like two magenta circular arrows. 
5. Now the Overhang arrow can be dragged to a new location to 
 increase/decrease the Overhang on just the one extension line.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V9.0
Function: DIMENSION

Ref: 001-7340649

KB Article ID# PL8010747

Contents

SummaryDetails

Associated Components