NC Controller Will Not Accept the '_' (Underscore) Character

2019-04-22T15:14:39Z

Summary


Details

A Mori Seki milling machine with a MAPPS III controller will not accept an "_" (underscore) character in the posted G-code output even inside of an operator message. Is there an easy way to configure Post Builder to replace all these characters from the operation or tool name with a "-" (dash) instead? Notice the underscore characters in the two operator messages below.

%
O1
G90 G80 G40 G17
(PROGRAM_TO_MILL_SIDE)
(END_MILL_.250_DIA)

T1 M6
M3 S4580
GO G54 X2.9394 Y-1.927
G43 Z0.5 H12
GO ZO.2
G1 Z0 F9.0
X2.9808 F18.0
G2 X3.1187 Y-1.8646 I0.3702 J-0.635
G3 Y-0.198 I-1.2049 JO.8333
G2 X2.9808 Y-0.1356 I0.2323 J0.6974 
Gl X2.9394

Solution

Below is the TCL code that will parse the "_" characters from the mom_operation_name and the mom_tool_name variables and replace it with a "-" character.


### 
global string_wo_underscores 
global mom_operation_name 
global mom_tool_name 
global mom_sys_control_out mom_sys_control_in


set co "$mom_sys_control_out" 
set ci "$mom_sys_control_in"


regsub -all {_} $mom_operation_name "-" string_wo_underscores 
MOM_output_literal "$co$string_wo_underscores$ci"


regsub -all {_} $mom_tool_name "-" string_wo_underscores
MOM_output_literal "$co$string_wo_underscores$ci"
###

When output the G-code file will look as follows.

%
O1
G90 G80 G40 G17
(PROGRAM-TO-MILL-SIDE)
(END-MILL-.250-DIA)

T1 M6
M3 S4580

Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V1855
Function: POSTBUILDER

Ref: 001-7889550

KB Article ID# PL8010742

Contents

SummaryDetails

Associated Components