Problem with Indexing Reuse Library Search on a LAN documentation server

2019-05-08T06:51:29Z

Summary


Details

If the customer default is set to a documentation server in the LAN, from client machine, we can only do search instead of creating index.

Solution

The index creation can be done in the server only. So, the grey of "Send to index builder" button is our design.


We have an environment to support the index creation from client to server: 
UGII_REUSE_INDEX_TMP_DIR


For example: 
Set UGII_REUSE_INDEX_TMP_DIR=\\sharedmachine\reuseTemp


Make sure the folder \\sharedmachine\reuseTemp can be read/write in the LAN.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 10_1809
Product: NX
Application: KDA
Function: REUSE_LIBRARY

Ref: 001-8271161

KB Article ID# PL8010740

Contents

SummaryDetails

Associated Components