Silent NX install reboots by default

2020-08-13T20:02:30Z

Summary


Details

--------------- 
After each silent install, the system restarts.



Solution


msiexec -h

Lets review WIndows installer options:

Windows ® Installer. V 5.0.17763.404 

msiexec /Option <Required Parameter> [Optional Parameter]

Install Options
 </package | /i> <Product.msi>
 Installs or configures a product
 /a <Product.msi>
 Administrative install - Installs a product on the network
 /j<u|m> <Product.msi> [/t <Transform List>] [/g <Language ID>]
 Advertises a product - m to all users, u to current user
 </uninstall | /x> <Product.msi | ProductCode>
 Uninstalls the product
Display Options
 /quiet
 Quiet mode, no user interaction
 /passive
 Unattended mode - progress bar only
 /q[n|b|r|f]
 Sets user interface level
 n - No UI
 b - Basic UI
 r - Reduced UI
 f - Full UI (default)
 /help
 Help information
Restart Options
 /norestart
 Do not restart after the installation is complete
 /promptrestart
 Prompts the user for restart if necessary
 /forcerestart
 Always restart the computer after installation
Logging Options
 /l[i|w|e|a|r|u|c|m|o|p|v|x|+|!|*] <LogFile>
 i - Status messages
 w - Nonfatal warnings
 e - All error messages
 a - Start up of actions
 r - Action-specific records
 u - User requests
 c - Initial UI parameters
 m - Out-of-memory or fatal exit information
 o - Out-of-disk-space messages
 p - Terminal properties
 v - Verbose output
 x - Extra debugging information
 + - Append to existing log file
 ! - Flush each line to the log
 * - Log all information, except for v and x options
 /log <LogFile>
 Equivalent of /l* <LogFile>
Update Options
 /update <Update1.msp>[;Update2.msp]
 Applies update(s)
 /uninstall <PatchCodeGuid>[;Update2.msp] /package <Product.msi | ProductCode>
 Remove update(s) for a product
Repair Options
 /f[p|e|c|m|s|o|d|a|u|v] <Product.msi | ProductCode>
 Repairs a product
 p - only if file is missing
 o - if file is missing or an older version is installed (default)
 e - if file is missing or an equal or older version is installed
 d - if file is missing or a different version is installed
 c - if file is missing or checksum does not match the calculated value
 a - forces all files to be reinstalled
 u - all required user-specific registry entries (default)
 m - all required computer-specific registry entries (default)
 s - all existing shortcuts (default)
 v - runs from source and recaches local package
Setting Public Properties
 [PROPERTY=PropertyValue]

Consult the Windows ® Installer SDK for additional documentation on the
command line syntax.

Copyright © Microsoft Corporation. All rights reserved.
Portions of this software are based in part on the work of the Independent JPEG Group.

You can modify restart behavior by selecting 1 of the following 3 options:


/norestart - Do not restart after the installation is complete


/promptrestart - Prompts the user for restart if necessary


/forcerestart - Always restart the computer after installation 


Msiexec is not Siemens software - it is Microsoft Windows software, so 
some of the features in the msiexec options list may not be supported by all 
Siemens software installs.

Siemens does *not* suggest to use /norestart unless followed by a reboot
elsewhere in installation script and before other software is installed.

It is important to have all Siemens software in a 'clean' state before additional
software is installed or other changes are made.




Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: SYSTEM
Version: V1847
Function: WNT_INSTALL

Ref: 001-7731897

KB Article ID# PL8010736

Contents

SummaryDetails

Associated Components