---------------
"ug_clone" utility is not triggered while exporting NX data through PLMXML
Solution
After updating the site pref using preferences_manager the problem was
resolved.
From a Tc shell:
preferences_manager -u=infodba -p=password -mode=import
-preference=PIE_IMF_FOR_CAD -values="NO" -scope=site -action=OVERRIDE
Additionally, the following prerequisites must be met:
1. NX Manager must also be installed.
2. UGII_BASE_DIR should also be set in the environment
3. Per final response to PR 2227688 Tc9.1.2.5, Tc10.1.1, Tc11.1 or higher must be used.
Notes