Finding "Out of Date" components in an assembly if "Precise Only" load option is used.

2019-06-12T17:23:05Z

Summary


Details

After loading NX assembly using "Precise only" revision rule load option, how 
do you find out if there is a newer revision of the same component in 
Teamcenter data base?
What indication can you expect to see in Assembly Navigator?



Solution

 Here is what you can do in NX to find out if there is a newer revision of the 
same component in TC:


 1) In NX configure the column "TC Information" in the Assembly Navigator (ANT) 
 2) Load your assy. using "Precise Only" revision rule. 
 3) Set NX Load Options to Latest Working 
 4) Go to ANT --> Right Mouse Button (RMB) --> Refresh Teamcenter Information, 
 you should see "!" for the components that have newer revision. 
 5) Select the component --> RMB --> Close --> Reopen



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: FILE_OPEN

Ref: 001-7752286

KB Article ID# PL8010729

Contents

SummaryDetails

Associated Components