To enable Add Component Dialog with Full options.

2019-06-12T17:22:53Z

Summary


Details

When adding a component, many options are at the bottom part of the Add Component 
 that dialog may be missing, such as Settings, Interaction Options.


How do you enable these options?




Solution

 In the top left of the dialog, click the round gear for Dialog Options --> 
 Add Component (More) to see the full complete options of the dialog.


If a user does nothing, Less/More is mapped to the role they use, either 
 Essentials or Advanced. However, if they change the UI Preference, that will 
 take precedence. Go to Preferences --> User Interface --> Options --> Dialog Boxes
-->Default Presentation Of Dialog Content --> More



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V12.0.2
Function: ASSEMBLY_MODEL

Ref: 001-7140251

KB Article ID# PL8010712

Contents

SummaryDetails

Associated Components