---------------
Sometimes the Datum Csys objects may be too large relative to the drawing views they are displayed in. How can they be resized?
Solution
Make the file where the Datum Csys features were defined the Work Part and Edit the parameters of the Datum CSYS. Expand the Settings panel and set the Scale Factor to a value that gives the desired results on the drawing.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: DRAFTING
Version: V1847
Function: DRAWING/VIEW
Ref: 001-7482504