Engraving- text - How to do single pass type text.

2019-05-15T15:34:02Z

Summary


Details

Planar Text operation. Need to do text on a cylinder.



Solution

In Modeling: 
To create text on a cylinder. 
Use application Modeling-Curve-Text. In the Text dialog Type-On Face. Select 
Cylinder face and add in an Offset if needed. Location on Face- Placement 
location- Curve on Face- select either end of cylinder diameter. In the 
Setting section toggle on Project Curves. OK the dialog. At this point you 
should have text projected on to the cylinder. 


In Manufacturing: 
Create a valid tool and a Variable Contour operation. In the Variable Contour 
operation select the cylinder as Part Geometry. Set Drive Method as 
Curve/Point. Select each spline curve as a single entity and do an Add New Set 
for each. Tool Axis will be Normal to Part. Generate path.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V10.0.2
Function: PLANAR_MILLING

Ref: 001-7589854

KB Article ID# PL8010701

Contents

SummaryDetails

Associated Components