---------------
How can a user of NX 10 get a listing of information with the Location and
Names of attached results files to an active Solution?
Solution
Users can invoke the following tool to get the Solution Result information:
Menu-Information-Advanced Simulation-Solution Result...
Example:
------------------------------------------------------------
SOLUTION RESULT INFORMATION
------------------------------------------------------------
Solution name : wave601
Expected results directory : V:\
Expected results base file name : wave601_s-wave601.op2
Expected results file : V:\wave601_s-wave601.op2
Actual results file : V:\wave601_s-wave601.op2
File size on disk : 2635057376 bytes
Created on : 4/13/2016 11:29:36 AM
Modified on : 4/13/2016 3:17:42 PM
Units : Inferred
Notes