How to add multiple lines of text as a PDF watermark

2019-05-15T17:21:12Z

Summary


Details

When exporting a PDF file, how can a watermark be created that has multiple 
lines of text?



Solution

 There is no way to create multi-line watermark text from inside NX. The cgm2pdf 
command line utility has to be used. 
This command line utility has an argument (-wfile) to allow a text file 
(*.txt) as input for the watermark. And if the text file has multiple lines of 
text, then so will the watermark. 
1.  Export the drawing to a CGM file. 
2. Create the watermark text file like the following: 
--------------------------------------------------------- 
#OPACITY=.3 
#SCALE=1.0 
#DIRECTION=HORIZONTAL 
#ANCHOR=5 
This watermark should have 
multiple lines of text.


--------------------------------------------------------- 
Watermark file instructions: 
A. Place text to be used for the watermark on an open line (no comment #). 
B. Make sure the text file has one <return> to create one empty line at the end 
of the file. 
Watermark options that can be used in the watermark text file are as follows: 
· #OPACITY=<number>, where <number> is a decimal number from 0 to 1. The 
default is .3. 
· #SCALE=<number>, where <number> is a decimal number. The default is the page 
size. 
· #DIRECTION=<keyword>, where <keyword> is given as VERTICAL, HORIZONTAL, or 
DIAGONAL. The default is DIAGONAL. 
· #ANCHOR= =<number>, where <number> is the anchor point given by a value. 
Allowable values are: 
 o 1 = Top left 
 o 2 = Top center 
 o 3 = Top right 
 o 4 = Center left 
 o 5 = Center 
 o 6 = Center right 
 o 7 = Bottom left 
 o 8 = Bottom center 
 o 9 = Bottom right 
 The default value is 5 (Center). 
3. Open an NX Command Prompt: 'Start-->All Programs-->Siemens NX 9.0-->NX 
Tools-->Command Prompt'. 
4. Run the cgm2pdf.exe utility using the following syntax: 
cgm2pdf.exe -wfile=<watermark_file> cgm_filename.cgm pdf_filename.pdf


I have used the entire path to all the files so they are found and used. 
For example: 
D:\NX9\NXPLOT\bin\pdf\cgm2pdf.exe 
-wfile=D:\user_files\watermark_text.txt D:\user_files\drawing.cgm 
D:\user_files\drawing.pdf



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: GATEWAY
Version: V9.0
Function: PDF

Ref: 001-7771896

KB Article ID# PL8010691

Contents

SummaryDetails

Associated Components