Creating a button for Measure type on Analysis Measure Distance Tool

2019-08-23T13:06:41Z

Summary


Details

--------------- 
On the dialog of Analysis Measure Distance, there are different types but you 
could create some popular types on a toolbar for your convenience if you wish.



Solution

 You can use Save Favorite to create your more often use type on Analysis 
Measure Distance as below:


When you are in the Measure Distance dialog, set the type you want then right 
click on the top bar, (Measure Distance) --> Save Favorite As.


You can also create more than 1 favorite on a toolbar. Do the following:


You can create your new Toolbar from Tools --> Customize --> Toolbars --> New 
then you go to Commands --> New Button --> Drag and Drag New User Command to 
this new toolbar --> Select New Command on this new toolbar --> RM -->Edit 
Action --> Set Type to Favorite --> Select your favorite --> OK, then repeat 
the step from Drag and Drop a new user command to this new toolbar --> Select 
the User Command --> MB3 --> Customize --> MB3 --> Edit Action --> Set Type to 
Favorite --> Select your favorite --> OK.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V8.5.3
Function: UI_TOOLS

Ref: 001-7203180

KB Article ID# PL8010683

Contents

SummaryDetails

Associated Components