How to make SPLM Licensing work when a Firewall exists on the server?

2019-08-21T12:16:06Z

Summary


Details

NX workstations remote from the Siemens PLM License Server are unable to get a 
license when a Firewall is turned on at the server. The Firewall is blocking 
TCP/IP socket communication between the Siemens PLM License Server and the NX 
workstations.



Solution

The easiest way for licensing to get through the Firewall is to add PROGRAM 
EXCEPTIONS to the Firewall on the server for the following licensing binaries. 
For example, assuming Siemens PLM Licensing is installed to the default 
location:


    C:\Program Files\Siemens\PLMLicenseServer\lmgrd.exe (license manager daemon) 
    C:\Program Files\Siemens\PLMLicenseServer\ugslmd.exe (vendor daemon)


Alternatively, if PORT exceptions need to be made as in the case of VPN, 
TWO ports would need to be added and opened for both inbound & outbound 
traffic:


    1. Port 28000 for lmgrd (default) 
    2. Static port for ugslmd (e.g. 28002) 






Notes and References

 Assign a STATIC port (variable by default) to the vendor daemon 'ugslmd' 
 by adding the PORT keyword to the VENDOR line in the license file, for 
 example:


 SERVER servername COMPOSITE=xxxxxxxxxxxx 28000 
 VENDOR ugslmd PORT=28002

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: SYSENG
Version: V1872
Function: SYSTEM_TOOLS

Ref: 001-7484093

KB Article ID# PL8010676

Contents

SummaryDetails

Associated Components