NX Static Constructors which may have been called before sufficient initialization

2019-05-24T11:44:04Z
NX Open NX System Administration

Summary


Details

The NX information window comes up and shows something like this: 
**************************************************************************** 
**************************************************************************** 
* This session had the following problems. * 
* Static Constructors which may have been called before sufficient * 
* initialization has been performed. Examples are trying to translate * 
* strings before the system has initialized the translation mechanism or * 
* declaring localization strings as file statics which construct during * 
* library load or looking up environment variables before ENV has been * 
* initialized. * 
**************************************************************************** 
**************************************************************************** 
File D:\workdir\reference\NX1003_5\src\syss\ug02\ind\System_L10N_Localize.cxx: line 407: File 
D:\workdir\Patches\nx1003_patch\src\ugutilsint\no\ind\exp_dlog_ui.c LOCALIZE: Localization can not be called from a file global static constructor for "Edit Single Interpart Expression"


The path to the File may vary with NX version. The path shown is NOT a valid location on the user's workstation.



Solution

Make sure that the environment variable UGII_CHECKING_LEVEL is NOT set. This environment variable is intended for NX development use only and may cause information to be shown that is not intended to be displayed to customers.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 732SP1
Product: NX
Application: SYSENG
Version: V10.0.3
Function: NXOPEN

Ref: 001-7918102

KB Article ID# PL8010656

Contents

SummaryDetails

Associated Components

Block/UI Interface Stylers Knowledge Fusion Menuscript NX Open - All Languages NX Open Python Open for C/C++ Open for CAE Open for GRIP Open for Java Pre-NX6 UI Styler SNAP UDO