Unable to select a datum axis when creating a dimension

2019-05-15T17:16:50Z

Summary


Details

While in a Sketch, a datum axis is unable to be selected while creating a 
Horizontal, Vertical, or Parallel dimension.



Solution

 If a Sketch dimension needs to be associated to a datum axis, use the 'Inferred 
Dimension' command instead.


The reason why a datum axis cannot be selected for a Horizontal, Vertical, or 
Parallel dimension is because these dimension types are point-to-point 
dimensions. Datum Axes in NX do not have a user-visible point.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V7.5
Function: SKETCHER

Ref: 001-6832631

KB Article ID# PL8010652

Contents

SummaryDetails

Associated Components